IP.ADDRESS

Description

This parameter is used to set the IP address of the drive for service port communication when IP.MODE is set to 1 for static IP.

Examples

Usage

IP.ADDRESS is only used when IP.MODE = 1. When setting up the drive with static IP, IP address must be set using IP.ADDRESS and subnet mask must be set using IP.SUBNET. IP.RESET can then be used to apply the specified IP settings.

Code

Set drive to be able to communicate with devices on 192.168.1.x subnet.

--> IP.MODE 1
--> IP.ADDRESS 192.168.0.1
--> IP.SUBNET 255.255.255.0
--> IP.GATEWAY 192.168.1.1
--> IP.RESET

Context

For more information on IP configuration, see Finding and Connecting to a Device.

Versions

Action Version Notes
Implemented 02-00-00-000

 

General Information

Type Read/Write
Units N/A
Range 0.0.0.0 to 255.255.255.255
Default Value 0.0.0.0
Data Type String
See Also IP.MODE, IP.SUBNET, IP.GATEWAY, IP.RESET

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

IP.ADDRESS

3013h

01h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

IP.ADDRESS

2202

89A

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

IP.ADDRESS

2202

Unsigned32

Read/Write

-